The only way to know is to identify symptoms of harmonics. Very often, if you recognize specific symptoms of harmonics, the problem has already created issues on your power system. The trick is to recognize “potential” symptoms and identify potential harmonic issues before they occur or to implement correction into the system design. Sometimes modeling and simple calculations will help identify the issues before they become a problem.
Simply stated, there are two basic concerns:
Equipment failure and misoperationThe following symptoms are examples of equipment failure and misoperation associated with harmonics on a power system:
Economic considerationsThe following are economic considerations that should be evaluated with regard to harmonics:
Power factor correction capacitorsApplying power factor correction capacitors requires special considerations with regard to harmonics:
Other significant issuesOther significant issues are typically raised with regard to harmonics. Interestingly, these issues are often not real problems but rather hype created by a lack of understanding of harmonics. Many “harmonic problems” are specification issues rather than real problems.
Harmonics in power systems result in increased costs and downtime. Get help from Eaton.
Depending on your electrical power system, there are a lot of places where harmonics can cause inefficiencies.
In a manufacturing setting, unmanaged harmonics can increase motor temperatures by 10 degrees to maintain output. This side effect can reduce the life of a motor by 50%. Distribution transformers can lose a full +1% of efficiency when carrying 100% harmonic current, and motors lose 0.1% efficiency with each 1% of harmonic voltage distortion. These losses can cause a dramatic decrease in the lifespan of fan and pump motors due to extra heating in the motor stator.
In a hospital setting, a large HVAC system with a 500 horsepower fan and pump load, running at 5% voltage distortion instead of 1%, can cost $15,000 per year at 10 cents per kwh. This is in addition to the costs of the reduced lifespan of the motors caused by the heating effects of the harmonic currents.
Learn and understand if you should expect harmonics on your power systems based on your loads and systems of harmonics.
Do you have additional questions or just want to communicate with someone well-versed in harmonics? We have experts ready to answer any questions you may have.