Go back to the main troubleshooting protective relays page.
For additional support
For additional manufacturer technical support, please contact 1-800-809-2772, option 4, then option 1 or use the email address, MRsupport@eaton.com.
Problem or maloperation in… |
Problem description |
Corrective action |
| Failure of time synchronization. | Check the following issues:
|
|
Failure of the TCP/IP connection. |
Check the following issues with your local IT:
|
|
| USB COM port is not visible on the PC. | It is not possible to connect PowerPort-E, Field Device Installer or some other application to the relay via USB. The corresponding USB port (e.g. COM 5) is not visible in the application. | Check the following issues:
|
| USB COM port visible, but no connection possible. | It is not possible to communicate with PowerPort-E to the relay via USB. The corresponding USB port (e.g. COM 5) is available and was selected correctly. | Check the following issues:
|
| Older protective devices with RS232: PowerPort-E does not connect via RS232. | It is not possible to establish a connection with PowerPort-E from a PC to the device via RS232. | Use a PowerPort-E version release 3.41 or higher. Starting from this release PowerPort-E supports a simplified creation of a serial connection. If your PC does not have a serial port, you need a USB-toserial-adapter that has been approved by Eaton. This has to be installed correctly. Verify that your cable is a zero-modem cable (please refer to the corresponding chapter). A simple serial cable does not have any flow control lines. A connection is only possible with a zero-modem cable. |
| PowerPort-E can not connect to the device. This has been possible before by using the same PC. | A connection between PowerPort-E and device has been possible before using the same PC. Now it is not possible to connect to the device. | Check the following issues:
|
| No communication (data transfer) with PowerPort-E possible, even though a connection has been established. | Port 52152 is being blocked by a firewall. | Check the settings of your firewall. You may require to unblock port 52152. |
Go back to the main troubleshooting protective relays page.
For additional manufacturer technical support, please contact 1-800-809-2772, option 4, then option 1 or use the email address, MRsupport@eaton.com.