How we generate and use electricity is changing. Energy-efficient appliances and gadgets consume less power. But as new energy vehicles become more popular, a new source of electricity demand is emerging.
With energy storage you can store your self-generated renewable energy for when you need it most.
The average home uses around 30% of all the energy generated by its solar PV panels. A residential solar energy storage system, like xStorage Home, can increase self-consumption to 70%.
As they become more affordable, more and more of us will choose to drive electric vehicles (EVs). With the xStorage Home system, you can charge your electric car on clean self-generated energy and avoid peak demand charges as well as high time-of-use tariffs. 
Home energy storage systems ensure that clean, renewable energy is used at times of peak demand, known as peak shaving. In the future, utilities could link up multiple individual energy storage units, thereby allowing them to defer investments while expanding grid capacity. Utility companies would not need to pass on the costs associated with grid investments, and energy storage system owners would get paid to help strengthen the grid— a win-win situation.
Using lithium-ion (Li-Ion) batteries from electric vehicle (EV) leader Nissan, integrated with our robust power control technology, xStorage Home comes as a single wall-mounted box, designed to energize your home seamlessly and reliably. The system can be easily programmed and controlled using a friendly user interface.
Once installed and set up by a certified installer, you'll have peace of mind knowing that by linking your solar array, your home and the grid, xStorage Home will help you optimize the consumption of clean energy, while reducing your electricity bills and providing power no matter what.